If the CODESYS WebVisu is implemented in the ctrlX PLC App runtime environment of ctrlX CORE, the device can display graphical user interfaces on connected HTML5-capable web browsers.
Integrated in the ctrlX PLC Engineering, the development of an IEC 61131-3 logic application as well as a classic or object-oriented visualization development becomes possible with one and the same development environment.
In CODESYS WebVisu, the controller features an integrated web server that makes image and variable data available in a data network. These data can be displayed on any HTML5-capable display devices with a standard web browser.
Project engineering with the editor integrated in the ctrlX PLC Engineering: The web server supports all visual elements of the ctrlX PLC Engineering on a controller with a ctrlX PLC App.
Visualization management via:
Specification of the display on the target device (update rate, width and height in pixels)
Universal modification of all masks via CODESYS Visualization styles
Management of actions by assignment of hot keys or mouse events
Setting of user groups for the graphic interface
Dashboard - Overview
New as of Version / Patch 3.6.3: Scalable Licenses
With the introduction of ctrlX AUTOMATION Patch 3.6.3, the licensing model for the CODESYS WebVisu App has been optimized and transitioned to scalable licenses.
What has changed?
The previous, universal standard license (R911411670 / SWL-W-XC*-COSY*WEBVISU***- NNNN) has been discontinued and is no longer offered in the Store.
Important Note for Existing Customers:
Previously purchased licenses (R911411670) will, of course, remain valid on your existing systems. For new projects or functional expansions from system version 3.6.3 onwards, please select the appropriate scalable license from the available portfolio.
Licensing and scalability
The CODESYS WebVisu app enables browser-based visualization access for applications running on ctrlX PLC.
Visualization licensing is based on the number of tags used within the visualization project. Tags are IEC variables used within the visualization. Depending on the application size and complexity, different performance classes are available to scale from small machine applications to large and plant-wide visualization projects.
License
Number of Tags
VISU 128 Tags
128
VISU 2K Tags
2,048
VISU 4K Tags
4,096
VISU 8K Tags
8,192
VISU unlimited Tags
Unlimited
Tags are IEC variables used within the visualization. Complex visualization elements such as tables or trend controls may require additional tags and are therefore considered when calculating the required license size.
The VISU 128 Tags is already included in the runtime system license and is therefore available by default as part of the ctrlX PLC App.
The VISU 2K Tags, VISU 4K Tags, VISU 8K Tags, and VISU unlimited Tags licenses provide increased visualization capacity for larger and more complex applications.
Prerequisites
Support
Related Links
Curious?
You can test many apps free of charge with a virtual control system provided by ctrlX WORKS.
Just downloadĀ ctrlX WORKS and follow this How-to
[link-button type="light" text="TRY IT NOW" target="_blank" href="https://community.boschrexroth.com/ctrlx-os-store-apps-oc2pqqwn/post/ctrlx-works-xOJLFLUiK4NGm5H"]
The Company
The CODESYS Group is one of the world's leading software manufacturers in the automation industry. At its headquarters in Kempten/Germany and its subsidiaries in China, Italy and the United States, the group currently employs 200 people. The CODESYS Group focuses on developing and marketing the manufacturer-independent IEC 61131-3 automation suite CODESYS and the associated product portfolio. CODESYS covers the complete software side of automation. Core products of the market-leading automation suite are the CODESYS Development System, the corresponding platform-independent control system CODESYS Control and the CODESYS Automation Server, the cloud-based industry 4.0 platform. The customers of the group, founded in 1994 by Dieter Hess and Manfred Werner, come from all areas of automation: manufacturers of industrial controls as well as their users or operators who automate or operate machines and systems with CODESYS.