Hello,
I am trying to control an L7NH servodrive with the motion app.
When I try to change the Motion operation mode (the switch in the top)to be able to start commisioning the drive, I receive two errors.
-Switch statemachine to Running failed
-Inconsistent system
I have set up the profile like so:
From what I can see, the drive I am using is a CANopen_over_ethercat drive so I made sure to select this.
I mapped the in/outputs like this:
I am not sure wheter or not I need to use the diagcode. I am not able to select it inside the drive.
The ethercat master is running like it should.
Also, when looking inside the datalayer I can see that data is coming in:
Could you help me solve the problem ?
Thank you in advance
Walter