I have recently upgraded a running ctrlX installation from V1.12 to V1.20. There are two dual axis IndraDrives with firmware MPM-20V26 and the Motion App is V1.20.5
If I setup a profile for either of the axis within each drive there are no issues. If I setup a profile for the second axis then I get the following error:
Each Profile is mapped to a different axis within the device.
Â
Â
Â