The avaiable DOK-XIO*** does not provide any information on the max current wiring of the XIO's common 24V and 0V and potential distribution terminals.
The 16 channel output module XI211116 docu says 0.5A per output and max. 4A per module. I do not know how many X211116 I can use without a potential reference module XI8241116 (8x24V, 8x0V). Also there is no current rating defined in ctrlX CORE docu R911405645 for the connector UD10 and 24V logic supply UL and peripheral supply UP.
Where is the document that shows how the supply lines (24V and 0V) must be wired when using the ctrlX IO?