Update ctrlX Drive with the right firmware to match V1.20

I want to upgrade my systems to V1.20 (CtrlX Drive with Core)

I found some topics similar on the Forum, but not exactly the same. I have ten similar systems and at least I want to connect the CtrlX Drive with Core as a slave to a S7-1500 (Master) with Profinet. (With the current version 1.16, I have never managed to get the Profinet to work.)

--> From the documentation ctrlX CORE Runtime Release Notes XCR-V-0120_EN (Ed 12) page 24

I read that for control XCR-V-0120 I need Drive Firmware AXS-V-0316 and AXS-V-0402

--> In document ctrlX DRIVE, Firmware Release Notes AXS-V-04 AV0402, page 5, I read that : Releases of version AXS-V-04RS only runs on generation 2 devices.

I have a ctrlX Drive with Core of type:

XCS2-W0023ARN-02AX3T0NNET-S03RSN0NNNN0NN

With a double axis of type:

XMD2 XMD2-W1616ANN-01AETT0NNNN-S0304N2NNNN0NN

All drives with MS2N single cable.

Does that mean that I must install Firmware AXS-V-0316 on my drives ?

And if yes, where can I found AXS-V-0316 ?

Regards,

CΓ©dric

Best reply by Drives_Uwe

Address to your technical contact at Bosch Rexroth to sort out if your device can be updated to version 04 providing him the serial numbers of your devices. Then he might help you with the upgrade or aks you to resend the devices.

View original
1 reply