Hello everybody,
I have got problem with ctrlX Drives. I have got:
- XCD2-W2323ARN-02AX3T0NNET-S0308N2NNNP0NN
- XMS2-W0006ANA-01NETT0NNNN-S0308N2NNNN0NN
All drives are with FWA-XD1-AXS-V-0308N-NN.02 firmware. XCD2 has got build-in ctrlX Core with RM22.03 firmware version. Motors are MS2N03. I have got a Cartesian Robot and I am using Motion Interface to control it.
The kinematics are working properly and here everything is good, but the problem is in switching from AF to AH/Ab. After the movement is finished, when I am using command "arKinCtrl_gb[Robot.GroupNo].Admin._OpMode:= ModeCoordAH;" or "arKinCtrl_gb[Robot.GroupNo].Admin._OpMode:= ModeCoordAB;" nothing happens - the drives are still under power in the AF state. The program is showing that the command has been executed and it looks like that:
But it is not true and the drives are still under power in AF state.
My colleague told me, that this problem occured after the update to RM22.03 version. Before everything was OK - he said.
Maybe somebody has got the similar problem or know the solution?