Where can I compensate the Motor Brake delay time.What I want is that the drive is enabled and on power before the brake is released.
I have a vertical movement with a big mass. When switching on (enabling) the drive I do not want the mass to drop, not even as small movement. I like to have it steady to get a smooth behaviour. What I see changing the delay times is that the drive ready bit can be shifted. Its also explained in the manual.
When I add 100 ms in the Delay time the Drive Ready Status bit is indeed delayed.Â
Where can I found the function to prevent the load to drop.
Â