Motor control frequency

Hi,

With indradrive, it is stated that using PWM frequency of 6000 Hz the controller's continuous current data of 8000 Hz apply. Is this the case also for ctrlX drive?

I intend to use velocity dependent PWM switching using switching frequency of 12 kHz. I need to know which continous current applies for this, since the project planning manual does not specify anything for 6 kHz.

Best reply by Drives_Uwe

Yes, please use the data specified for 8 kHz PWM.

View original
1 reply