EAL4 package for LabVIEW cRIO

Hello, I want to control a Rexroth device via LabVIEW using the EAL4 package. I've installed via VIPM and could build a simple project with a .vi running on the pc. But, I want to control the device in the cRIO, the issue is that When I deploy a .vi from eal4 library, the .vi is corrupt saying "Constructor node: node not supported in current target error". Do I need to install more software on cRIO to make it work ?

I'm using cRIO 9045 with LabVIEW 2023.

ย 

3 replies