I have ordered two drives, one single axis and one double axis and want to do a drive simulation while I am waiting for the hardware. My issue is to enter the correct device information to get an accurate representation of my system and the correct control section/firmware. My drives and motors are:
Single axis:Â XCS2-W0054ARN-02AETM5NNNN-S04RSN2NNNN5NN Runtime version: S04RSN
          - Motor: MS2N07-C1BRN without brake
Double axis:Â XMD2-W2323ANN-02NETM5NNNN-S04RSN2NNNN5NN Runtime version: S04RSN
          1st motor: MS2N06-B1BNN without brake
          2nd motor: MS2N04-D0BQN with brake
I have come this far in the setup and want to know if it is correct:
Please let me know which information is needed for the respective drives/motor combination.
Â