Accuracy of encoder velocity ACUROlink Advanced type -CS- (20Bit singleturn)

What is the accuracy of the actual velocity value (S-0-0040) and also for the SMO-speed value (P-0-3258) using a MS2N motor with ACUROlink Advanced type -CS- (20Bit singleturn) together with a IndraDrive HCS01.1 ?

(for the ctrlX SENSE there is 6% for the safe speed.) But at the ACUROlink is nothing for the speed. Just the system accuracy.)

I only saw the following information in the Online-Docs: The velocity of the ACUROⓇlink encoder is recorded at an interval of 1 ms with a tolerance of ±0.5 %. The resulting tolerance of the actual value for the velocity has to be taken into account for the risk assessment at the machine!

1 reply