Many of the Rexroth CAD files that are available are only available as 3D .stp files that cannot be used in 2D CAD packages, such as AutoCAD. This makes panel layout design difficult for 2D CAD programs as the dimensions must be created manually from manual information.
FreeCAD is an open-source 3D CAD package and has the ability to convert views of 3D .stp CAD files to 2D .dxf files.ย ย
The process isn't exactly a one-click process so I created some instructions, see the attached pdf.ย I'm not sure how dependent my instructions are on the versions of software that I have, but hopefully this can guide you to create 2D CAD files until the decision is made to make 2D CAD files part of the official, public documentation.
In the mean time, maybe you can use these that I already created, attached in a zip file:
XLL1_1WG401M0G-0210NNNNN-NNNNNN - this is an error, it is actually the XLL1-1NG402M0G-0050 in the drawing.ย Same for the 3D .stp file in the Media Directory.ย The source 3D file is named for a large product even though the smaller one is in the drawing.
XMV1-W0210ANC-xxNETT0NNNN
XMS1-W0150xxx-xxNETT0NNNN
XMS1-W0030xxx-xxNETT0NNNN