Customer is asking if they can save & write the log data and PLC project into the inserted micro sd card during operation. Is there any example or how-to ?
save & write the log data and PLC project on the µSD
Best reply by TheCodeCaptain
Hi Sophie,
you can read/write from the PLC or other apps like NodeRED to the memory card or usb-stick by using this path:
/media/mmcblk1p1/testfile.txt
The name of your device could be different and can be found in the ui under Settings-->Storage.
The PLC boot project is saved in the active configuration which is not on the memory card.
Find attached a plc example.
ROGRAM FileWriteAsync_PRG
VAR
fbFile: CXA_FileAsync.IL_FileAsync;
fbFileWrite: CXA_FileAsync.IL_FileWriteAsync;
filename: STRING := '/media/mmcblk1p1/testfile.txt'; // /var/snap/ctrlx-node-red/current/solutions/activeConfiguration/plc/run/linux-gcc-aarch64/data/myfilename.txt
itestcase: UINT := 0;
writebuf: STRING(500);
writebuflen: UDINT := 500;
writelen: UDINT := 0;
END_VAR
CASE itestcase OF
1: // open the file
fbFile(Enable:=TRUE, FileName:=ADR(filename), Mode:=IL_FILE_ACCESS_MODE.AM_WRITE);
IF fbFile.InOperation THEN
itestcase := itestcase + 1;
END_IF
2: // write the file
writebuf := 'BoschRexroth$R$NCtrlX Automation$R$NCXA_FileAsync$R$N';
writebuflen := IL_LEN(ADR(writebuf));
fbFileWrite(Execute:=TRUE, FileHandle:=fbFile.FileHandle, BufferAddr:=ADR(writebuf), BufferSize:=writebuflen, BytesWritten=>writelen);
IF fbFileWrite.Done THEN
fbFileWrite(Execute:=FALSE);
itestcase := itestcase + 1;
END_IF
3: // close file
fbFile(Enable:=FALSE);
If NOT fbFile.Shutdown AND NOT fbFile.InOperation THEN
itestcase := 0;
END_IF
END_CASE
IF fbFileWrite.Error OR fbFile.Error THEN
; // post some error
END_IF4 replies