Hello,
I have two issues with the microSD card on ctrlX (version 2.6 LTS):
1. An error occurs when trying to format the card to FAT32 or Ext4, even though mounting and formatting work well for USB drives.
a. error for Ext4
Format media
Task 'format' failed for media 'mmcblk1p1'. Reason: medium formatting '' failed: command: /snap/rexroth-deviceadmin/4176/sbin/mkfs.ext4 -F /dev/mmcblk1p1, Error: exit status 1
b. error for FAT32
Format media
Task 'format' failed for media 'mmcblk1p1'. Reason: medium formatting 'B4C3-D172' failed: command: /snap/rexroth-deviceadmin/4176/sbin/mkfs.vfat -F 32 /dev/mmcblk1p1, Error: exit status 1
2. After writing data to the microSD through Node-RED, I can read the data, but once I remove the card (of course, after triggering "Remove Safely"), the data is cleared and not visible on the PC.
Saving data from my PC to the microSD works well, so it's not an issue with the microSD card.
Unfortunately, I am unable to attach files to the forum after update. If needed I can send system report directly.
Thank you in advance for your help.