I have node-red app installed and licensed in a CtrlX core. it works. however when I tried to load a new node of "node-red-contrib-ui-led" I got an error of failed to install that node. then I viewed the log file into the details and got this message
see the attached log file. it looked like internet connection or setup issue.
Ā
here is what and how I have tried to make it work.
1. used it in the office. I have been using a company issued laptop and had the ctrlX(192.168.1.1) connected to the internet port(192.168.1.100) of the laptop and used wifi to get internet connection.it didn't work. then I set up a port forwarding for WIFI to use the fixed same IP address of WIFI(a different IP addess range). it did not work as well.
2. based on some suggestions from google I setĀ theĀ NODE_TLS_REJECT_UNAUTHORIZEDĀ environmentĀ variableĀ toĀ '0'. it still didn't work.
3. I tried to do the same at home and got the same error. then I set the IP addessed of CtrlX core and laptop to the same range of internet WIFI router at home and had two devides connected to the router directly. also switched off the VPN and turned on DHCP for the ipv4 of eth0. it didn't work.Ā
Ā
is the laptop setting blocking the registry website? what would be the best way to set the system and get a node downloaded? please let me know if there is a way to get it worked in the office since in the future we will mostlikely to support a customer from the office.
Ā
Thanks,Ā