Hi,
We have an issue with a image update on a brand new ctrlX CORE X5. (Version 4.4.0)
The Flash log file says:
2023/01/01 00:01:05 Checking if secureboot is enabled
2023/01/01 00:01:05 SecureBoot Enabled on system
2023/01/01 00:01:05 Checking if SbatLevels of image are compatible with system ...
2023/01/01 00:01:05 Fail: SbatLevels of provided image incompatible
2023/01/01 00:01:05 ERROR
2023/01/01 00:01:05 version of 'grub' you are trying to install too low [system: 2][install: 1]
The rescue.log file says:
-- Boot 7260430464463 --
RescueSystem: 2023/01/01 00:00:26 updater: Rescue System Version: v1.1.16
RescueSystem: 2023/01/01 00:00:26 updater: BootVar /dev/sda1 mounted to /boot
RescueSystem: 2023/01/01 00:00:26 config: '/boot/rescue/rescue.toml' file found, reading parameters
RescueSystem: 2023/01/01 00:00:27 web: start server on port 80
RescueSystem: 2023/01/01 00:00:27 updater: target device /dev/mmcblk0 available. continue..
RescueSystem: 2023/01/01 00:00:27 updater: start auto image flash with rexroth-arch02.ova image
RescueSystem: 2023/01/01 00:00:27 updater: clearing target device..wait..
RescueSystem: 2023/01/01 00:00:27 updater: target device cleared. continue..
RescueSystem: 2023/01/01 00:01:05 updater: auto image flash failed. error: exit status 20. continue..
What we already tried was to add a rescue.toml file with preclean = true, but still we cannot load the new image.
Anyone any suggestions?
Thanks