Hello,
I would like to connect ctrlX Core-M-X3 to Siemens PLC via Profinet.
I know that there is Profinet Device App and there is even short tutorial where XF23/XF24 ports are used - LINKย
But is it possible to use those ports with Codesys Profinet Device in ctrlX PLC Engineering? I added the Ethernet adapter there and then the Profinet Device and I wanted to chose network interface and I could not pick the XF23/XF24 ports.
Is it possible to have ctrlX Core as Profinet Device with Codesys add-on? Is there any tutorial how to do it?
Best regards, Filip
ย