04/29/2024
HowTo

Extend WebIQ Designer features with Add-On

History

  • 2026/02/12 Version 1.7

    • Add Text List Manager v1.0

    • Setup scripts converted from VBScript to more powerful PowerShell

  • 2026/02/05 Version 1.6

    • Add Unit Class Manager v1.0

  • 2026/02/05 Version 1.5

    • OpcUA check repaired

    • 2nd Add On Recipe Template Manager

    • introduction videos added

  • 2024/04/29 Update to version 1.2d

NOTE: The cx-select and cx-recipe widgets are included in the cx-Visual package, which is currently being released. Send a private message to HMIGuide if you require a preview version.

Introduction

WebIQ Designer is a powerful tool to create HTML5 machine visualizations. Nevertheless, the following functions are still missing:

Variable Manager

  • Important variable attributes clearly listed in one table

  • Editing an attribute of multiple variables with one click, e.g. set communication interval for all selected variables.

  • Cross reference list

  • OpcUA variable check

    • Variable still exists in the PLC?

    • PLC Data type changed?

Recipe Template Manager

  • Sorting of recipe items

  • Grouping of recipe items

Text List Manager

  • GUI to create Global text lists (with optional images)

  • The widget specific text lists of iq-select, creates doubles of identical text lists

The WebIQ Add-On (see attachment), developed by Bosch Rexroth, has these features. It is a standalone HTML5 page that is displayed in the web browser. The WebIQ Connect API documented on https://www.smart-hmi.com is used to implement the features.

Startup

  • Download and unzip the attached file.

  • Open addon\index.html to read

    • installation documentation

    • Variable Manager documentation

    • Recipe Template Manager documentation

  • Watch the videos to get a first impression of the add-ons.

    • Read documentation

  • Variable Manager

Recipe Template Manager

  • Unit Class Manager

  • Text List Manager

4
install-webiq-addon-v1.5.zip
1.04MB
install-webiq-addon-v1.6.zip
1.49MB
install-webiq-addon-v1.7.zip
1.79MB
Types
How-to
Products
HMI
Markets
Manufacturing
Assembly Lines
Building Automation
Logistic
Packaging
Printing
Production Machines
Robotics
Semicon & Electronics
Sonstiges