01/29/2024
Balluff | BTL Linear Position Sensor | ctrlX CORE | Connectivity

Set up a Balluff BTL Linear Position Sensor with ctrlX CORE using EtherCAT

Introduction

This How-to describes the integration of a Balluff Linear Position Sensor BTL34TC with EtherCAT interface into ctrlX CORE. It shows possibilities for configuration and diagnosis. Other Balluff Linear Position Sensors from BTL7-V50E-Series can also be commissioned in this way.

Requirements 

Hardware

Used Software

  • Rexroth PLC app 3.6.2

  • Rexroth EtherCAT Master app 3.6.2

  • ctrlX I/O Engineering and PLC Engineering 3.6.2

Step-by-Step guide

New Project 

  • Open ctrlX CORE user interface in browser.

    ctrlX CORE User Interface
  • Add EtherCAT master by clicking [+] in EtherCAT > Configuration.

    EtherCAT / Add EtherCAT Master / [+]
    EtherCAT / Add EtherCAT Master / [+] / Add
  • Open ctrlX I/O Engineering by double klick on the ethercatmaster

    double click ethercatmaster

    ctrlX I/O Engineering

    Open New project.

    New Project

Install device description

EtherCAT-Device configuration

  • Add Device to EtherCAT-Master by right-click in the device tree on ethercatmaster > Add Device:

    EtherCAT Device Configuration
  • Choose the right ESI (device description) for your device from device catalog > Add Device:

    Add Device
  • The position sensor is now ready without any configuration
     

    Position Sensor

Port Configuration

  • The BTL7-V50E-... corresponds to the profile for absolute linear encoders and is configured as a modular device. The transducer represents a virtual module carrier that has 16 slots for magnets. Various virtual modules that specify which data is assigned to the respective magnet can be inserted into each slot. This defines the data mapping, the assignment of the measurement data in the output. data.

    Technical Overview
  • To configure the behavior of the magnet, right click on Magnet_x > Plug Device

    Plug Device


    Choose  module > Plug Device 

    Measurement Modules
  • For diagnosis, error messages can be added with optional information about the temperature:
    right click on Device_1 > Plug Device > Choose  module > Plug Device 

    Diagnosis Module
  • Configure the number of expected magnets to receive an error message in case of a missing magnet.
    Use the flexible mode, if the number of magnets changes while the application is running.

    Magnet Numbers

Diagnosis

  • Direct information about the magnet can be seen in the process data of the corresponding magnet.

    Diagnosis PD2



    Diagnosis PD I
  • An optional module for error messages can be plugged into Device_1. Now an error-bit is shown direct in the process data.  

    Errors Codes PD


    The error register is also shown in the CoE 

    Errors CoE 2
  • Error codes and meaning

    Error Codes 2
  • The status of the magnets can also be seen in the CoE online data:

    Errors CoE

Parametrization

  • The BTL7-V50E-... can additionally be used as a cam switch. For this purpose, four cams are available for each magnet.

    CAM I


    There are four parameters available to configure and define each cam.

    CAM II


    Configuration can bee done via CoE:

    CAM III


    It is also possible to configure via startup parameters:

    Configuration
    CAM IV
  • The work area can be configured in the same way:

    Work Area

Related Links  

The Company 

Your partner for success in automation

Balluff is a leading supplier of high-quality sensor, identification and image processing solutions, including network technology and software for all automation requirements. We adhere to our motto “innovating automation” as an agile developer and technological pioneer. And we always act sustainably. We deliver innovative solutions to increase your competitive ability. Our consistent digital orientation drives our joint progress, and our innovative spirit factors directly to your success factor. Family-run for more than 100 years, Balluff today employees around 3600 employees worldwide who are committed to the highest quality standards for your success. As a future-oriented company, we are also dedicated to the development of digitalization and IIoT applications for an increasingly digital and networked world. You can rely on us, our promises, our commitment and Balluff quality – all in the name of a mutually beneficial partnership

1
Types
How-to
Products
IO