11/13/2024
How-to | Safety

Send ctrlX SAFETY Diagnosis to ctrlX CORE logbook

The function block SAFEX_Send_Diag_to_CORE_xVxx gets the diagnostic information from the function block SAFEX_Diagnosis_xVxx (see: Get ctrlX SAFETY Diagnosis at ctrlX CORE (over EtherCAT)) and send the error text to the ctrlX-CORE-Diagnostics-Logbook.
However, only errors that are related to the inputs and outputs of the ctrlX SAFETY are analyzed and send to the ctrlX CORE Diagnostics Logbook. 


The library CXAC_Diagnostics is necessary. So, check whether it is included in the PLC project or add it if not:

Import the attached function block:

Import the function block

Integrate the function block into your program, see example:

Example for the application of the Functionblock SAFEX_Send_Diag_to_CORE_xVxx

If than, e.g. an Plausibilty error occurs:

Example for an Plausibility Error

The Error is logged in the Logbook and can be confirmed with a reset:

Error entry in the ctrlX CORE Logbook

 

PS: How-to created by Dias; Current contact: Thoomas

1
SAFEX_Send_Diag_to_CORE_1V00.xml
57.54KB
Types
How-to
Products
Safety