04/26/2024
How-to | Safety

Get SAFEX-C.1x diagnosis information on the ctrlX CORE (over EtherCAT)

This PLC function block reads the diagnosis information from ctrlX SAFETY controller SAFEX-C.1x and monitors the communication.

It exists in two types:

  • FB-Type1 (original): FB β€œSAFEX_Diagnosis_1V04β€œ for firmware/FPGA <= 1.0.1.53/221 with ENG-Version <= 1.8.3.10207 (official version since September 2024)

  • FB-Type2 (extended): FB β€œSAFEX_Diagnosis_2V00” for firmware/FPGA >= 1.0.1.65/227 with ENG-Version >= 1.8.7.10917 (new official version since April 2026)

If you use a SAFEX-C.1x as an EtherCAT SubDevice with ctrlX CORE as EtherCAT MainDevice you need the status information from the safety controller. You find this information at the Functional Outputs from SAFEX-C.1x as Input for the PLC:

Status information and Functional Outputs of SAFEX-C.1x

  • FB-Type1 and 2: The first five bytes include the Mode (device status), the LiveCounter, the ErrorCode etc. of the SAFEX-C.1x. To make the access to this information easier you can use this function block.

  • FB-Type2 provides this information too and additional diagnosis information like CRC, FW-version etc.

Make sure that the β€œAdditional diagnostic” is activated in the properties of the SAFEX-C.1x for both FB-Types:

In addition for FB-Type2 the β€œAdd Non-Cyclic Data” must be activated as well.
The functionality and how to enable the new feature is described in the manual (Remark: will be officially released soon, here the preview:)

Description of the functionality in documentation (part of)

Note: For elements 4, 5, 6 (CRC_PMT-), "0" is supplied (not used).

For better use of real names, a user type (ENUM) is used for FB-Type2 for the Non-cyclic Data:

ENUM-type for the Non-cyclic Data

Β 

Note: There is nothing to program in the SAFEX-C1.x; but in the ctrlX PLC project only.

How to program it within user’s PLC program?

Step 1: Import the attached function block* for either FB-Type1 (SAFEX_Diagnosis_1V04.export) or FB-Type2 (SAFEX_Diagnosis_2V00.export)

Note: After downloading unzip the attached *.zip-file before import the *.export-file.

Import the function block (both variants)

Note: *The import-file for FB-Type2 contains not only the function block itself, but also an easy program example for the implementation (optional proposal), see below Step 2b.

Data-import of SAFEX_Diagnosis_2V00.export

Step 2a for FB-Type1: Call an instance of this function block

Call and configure the function block (variant 1 and 2)

You need the start address (pointer) of the FunctionalOutput as an Input, in this example ADR(%IW40) (see screenshot above).

With FieldbusType you distinguish between EtherCAT (FALSE, default) or PROFINET (TRUE).

The function block gives you as Outputs:

  • Mode:Β  Β  Β  Β  Β  Β  Β  Β  Β  Β  Β Device status: 1 = Init, 2 = Self-test, 3 = BusInit, 4 = Run, 5 = Stop, 8 = RunIntern; 6 = Fatal Error, 7 = Alarm

  • Device status as BOOL-signals: FatalError, Alarm, RunIntern, Run

  • LiveCounter:Β  Β  Β  Β  Β  Β As long the value counts the communication is OK
    ErrorCode:Β  Β  Β  Β  Β  Β  Β  Includes the ErrorCode in case Warning or Alarm is activeΒ  Β  Β  Β  Β  Β  Β 

  • CommunicationOK:Β  If this bit is TRUE, then the communication is OK

Step 2b for FB-Type2 only: Call an instance of this function block

The function block is also embedded in an easy program example:

Implementation-example of FB SAFEX_Diagnosis_2V00

In addition for FB-Type2 (compared to FB-Type1), the function block has two further inputs and outputs:

  • FunctionalInput: Β Β Β Β Β Β Β Β Β Β  start address (pointer) of the FunctionalInput as an Output, in this example ADR(%QB48) (see screenshot above)

  • NonCyclicCommand: ENUM (integer), Command/Request for the non-cyclic data to be read

  • NonCyclicResult: Β Β Β Β Β Β Β Β  ENUM (integer), Result of the non-cyclic data (such as an acknowledgment when reading)

  • NonCyclicData: Β Β Β Β Β Β Β Β Β Β Β  Value of the read non-cyclic data

Interface of Functional Inputs for non-cyclic data

Interface of Functional Outputs for non-cyclic data

In the example program, all Non-Cyclic Data are stored in an array:

All non-cyclic data of the SAFEX-C.1x (array)

PS: How-to created by Dias (FB-Type1); extension (FB-Type2) and current contact: Thoomas

1
SAFEX_Diagnosis_1V04.zip
3.14KB
SAFEX_Diagnosis_2V00.zip
5.12KB
Types
Example
How-to
Products
Controls
PLC
Safety