09/08/2025
How-to | HMI | WebVisu

HowTo change language with unit conversion in CODESYS WebVisu

Introduction

Text translation works as follows:

  • Every static text, which you enter in any screen is added to a table (POU> GlobalTextList)

  • In this table you define the translation for the different languages

  • When no translation is defined for the selected language, the original text is shown

  • Table can be exported/imported for external editing

Unit conversion works as follows:

  • The PLC codes always calculates using the base unit (e.g., meter)

  • The HMI converts the PLC's base unit to the desired unit (e.g. inch)

    • Hmi reads value from PLC:

      Convert from m to inch. Example: m2inch.convert(rValue)

    • Hmi writes value to PLC:

      Convert from inch to m. Example: m2inch.reverse(rValue)

Features of the ctrlX PLC Engineering example project

  • Languages: English (en), German (de) and French (fr)

  • Translation of static and dynamic text (=text provided in string variable)

  • Linked units:

Units of

length

temperature

PLC

m

°C

language de,fr

m

°C

language en

inch

°F

  • When switching a language

    • text is translated

    • unit values are converted into the unit values of the language

    • unit strings are converted e.g. (m => inch, °C => °F)

    • decimal places of the value are adapted to the unit needs

Basic implementation steps

  • Define languages and translate texts

  • Define unit conversion rules

  • Connect unit conversion rules to edit fields

The attached PLC v2.6.6 project, contains the below shown visualization with more documentation.

Related Links

set-language-units.project
750.11KB
Types
How-to
Products
PLC
HMI
Markets
Manufacturing
Assembly Lines
Building Automation
Logistic
Packaging
Printing
Production Machines
Robotics
Semicon & Electronics
Sonstiges