History
13 March 2025
Update to WebIQ 2.15.10, Update of WebIQ widgets (names changed)
10 May 2023
cx-osci: increase from 2 to 5 x,y curves, add css modifiers hidden, invisible
cx-char: add css modifiers hidden, invisible
update PLC program
27 Apr 2023
Initial release
Prerequisites
WebIQ Designer version 2.15.10 or higher for example project
Widget packages can be used in older WebIQ versions
Basic knowledge of WebIQ Designer
Plc Engineering 1.12.9 or higher
Basic PLC programming know how
Basic JSON know how (optional, when you want to change any chart setting)
Introduction
WebIQ contains a trend element which allows to show trend charts. The smallest recording time is limited by the smallest communication update time. Therefore, with this mechanism you can't display data which changes in a few msec or even less. With this example you get an oscilloscope functionality, where the PLC program:
Records data (in every PLC cycle)
Transfers configuration & data via CSV & JSON strings
Sends it via OpcUA to WebIQ.
Communication is like a REST API, via command & status strings
In WebIQ the plotly.js library is used to display the data.
Plotly is open-source graphic library (MIT license). Here a list with some features of plotly:
bar, line, pie, scatter, ... charts
zoom & pan functions
configuration of axes, colors, fonts, positions,....
Online graph maker, which allows you to define & display data and configure the appereance of the chart.
This example is based on 3 elements:
WebIQ package: package-plotly-basicÂ
WebIQ package: cx-plotly (provides WebIQ controls to use the plotly functionality)
PLC example program, which provides x,y data to display and optional configuration strings for plotly
Hint: You should read https://plotly.com/chart-studio-help/zoom-pan-hover-controls/ to get familar how to zoom and pan a chart.
Features
graphical and table display of recorded data
widget cx-chart (bar, pie, line)
widget cx-osci (scatter)
two data references/ PLC variables
two y axes with different scales
configurable titles for all axes
configurable names of data references
selectable line style (line, markers)
zoom, pan
show/hide of data references
Helpful links
Plotly home page:Â Â https://plotly.com/nodejs/
Plotly online graph maker: https://chart-studio.plotly.com
Usage of WebIQ demo project Demo-Oscilloscope-Chart-v*.zip
There are 4 tabulators in the WebIQ project.
Info: provides basic information on the usage of the program
Oszi data simulated in HMI: displays data, calculated in WebIQ (to allow testing without PLC)
Oszi data from PLC: displays data, calculated in PLC
(PLC must be connected and run, Check OpcUA settings for a successful communication)Chart data simulated on HMI
Use functionality in your project
WebIQ
Add package package-plotly
Add package cx-plotlyÂ
Insert widget from folder cxGraph and fill in necessary items
To optimize communication, you can set the "Update Interval" of all cx-osci items to "Read once". Only the "Message item" needs cyclic update (e.g. 200ms)
Plc
Open cx-osci-PLC-example.zip
Library StringUtils must be included in Plc project
Adapt start trigger and recorded data in PLC_Prg
Adapt axes names and titles displayed in the chart in call of mSetup in PLC_Prg
Configuration of plotly
If you want to change any of the predefined settings, adapt plotly data, layout and configuration settings JSON string, in PLC_Prg.mSetup.
Alterntively you can create the string in WebIQ
To be sure, that the JSON string is formated correctly, use a JSON editor. (e.g. JSON Online editor).
You can use Plotly Online graph maker to test the possiblities of plotly.
ATTENTION:
You can use WebIQ local variables, to display string in the chart. Ensure, that the content of the local variable does NOT contain any double quote ("), otherwise you get an error while parsing JSON string containing this variable. => chart can not be displayed.
PLC example project contains
Hints: for implemention data recording and string creation
String>IL_String: FB for performant string creation
String>ReplaceAOut: Function for string replacement (to replace variables in a JSON string)
Requested features next versions
Â