11/27/2025
Technote

How the ctrlX PLC License Metric calculates

Introduction

The following TechNote will explain how the limits for the different ctrlX PLC licenses are applied and which ctrlX PLC license I may need in the end for my project.

Criteria's

The ctrlX PLC license depends on 3 different criteria’s:

  • number of PLC Tasks

  • number of used CPU cores for the ctrlX PLC

  • Amount of IO data used in PLC project

PLC license overview

PLC Tasks

From version 3 on, there will be no limitation of PLC tasks anymore.

CPU Cores

The PLC program can run on one or multiple CPU cores. If you need to split your program on more than one CPU because of performance reasons, you need at least the "Advanced" license.

IO Data

The number of IO data is a result of the sum of all the data which is configured underneath the

  • DataLayer_Realtime’ Node or underneath the

  • Codesys field bus Add-Ons

Please note: By default only the variables are counted, which are actually used in the PLC program.

ctrlX PLC Engineering - IO example

For using the motion functionality of an axis there is no need to add the axis under the "DataLayer_Realtime" node, because the ctrlX MOTION App and the Motion Interface directly communicate via the ctrlX Data Layer. This means that the parameters related to the ctrlX MOTION App don’t need to be added (e.g. Drive Status Word, Master Control Word, Position Command Value, Position Feedback Value, Probe Input Value, etc.)

Only non-motion parameters, which should be processed in the PLC program in real time must be added. If you want to monitor for example a motor temperature in the PLC, then the drive parameter must be added.

In the first step you need to add it in the cyclic process data via the IO Engineering. Below you can see the configuration of one drive, where the default parameters were extended by the motor temperature.

ctrlX IO Engineering - drive default parameter configuration
ctrlX IO Engineering - default parameter configuration extended by the motor temperature

This configuration from the ctrlX IO Engineering can be imported in the ctrlX Motion App. All the variables related to the motion App will show up in the Axis profile and must not be configured underneath the "DataLayer_Realtime" node.

ctrlX OS web UI - automatically imported configuration in the axis profile

Only the motor temperature from the example above must be added underneath the "DataLayer_Realtime" node and hence will increases the amount of IO data.

ctrlX PLC Engineering - add motor temperature to "DataLayer_Realtime" node

FSoE telegrams don’t have to be considered. They are exchanged between FSoE Master and Slave directly and won’t be processed via the PLC. However, the PLC normally needs to read out at least status information, e.g.:

  • Status of safe inputs, like e-stops, safe door contacts, etc.

  • Status of the safe mode of the drives

  • etc

This information needs to be mapped into the PLC program and will in the end increase the amount of IO data. 

Information of used IO data for IO module

This following example shows, where you can find the bit width in the process data image for your IO module.

E.g.: ctrlX I/O, Analog Input Terminal XI332204, 4-channel, 0 to 20 mA, 16 Bit, Bipolar

General technical data - ctrlX AUTOMATION – Product information

Online documentation - example of ctrlX IO

Check the actual license status 

The actual license status can be checked by clicking on the controller and select the tab <License Overview>.

ctrlX PLC Engineering - actual licence status

 In the simple example from above the following configuration was used:

  • 2 ctrlX DRIVES

    • a 2 Byte parameter was additionally configured on one of the drives

  • 1 Bit digital input

  • 1 Bit digital output

This adds up to 3 Byte IO data

Please note: the count is bit-wise, but rounded to a Byte value.

 

Example of a Robot Application

The application consists of:

  • 2 x cartesian robots (6 axis in total)

  • 1 belt axis

  • 1 Safety PLC

  • 1 bus coupler with 6 modules (details see screenshot below)

ctrlX PLC Engineering - example license count of a robot application

In total 30 Bytes are used in this example application, which are distributed like this:

  • 5 Bytes of IO modules

  • 0 Byte of Fieldbuses 

  • 24 Bytes Non-motion drive parameters (e.g. S-0-0135, S-0-0240, S-0-2057/2058)

  • 1 Byte Communication with Safety PLC

Summary

Hence the amount of IO data consists mainly of:

  • The used IO modules

  • Fieldbus communication (Profinet, EthernetIP, ModbusTCP, etc.)

  • Additional non-motion related drive parameters, which are configured cyclically

  • Data exchange between the PLC and a safety PLC

Related links

1
Types
Technote
Products
PLC
Markets
Sonstiges