09/02/2024
How-to | Siemens TIA-Portal™ | ctrlX DRIVE

ctrlX DRIVE with Siemens TIA-Portal™ CPU SIMATIC S7-1200 or S7-1500

Connection of ctrlX DRIVE to Siemens SIMATIC controllers like SIMATIC S7-1200 or S7-1500.

We offer function blocks to drive controlled positioning or parameter access from a Siemens SIMATIC controller over PROFINET to a ctrlX DRIVE or Power Supply.

The function blocks are provided with an example program, parameter file, device description file and documentation to get it quickly running.

e.g.

  • FB_TIA_PN_DCP_cXD function block to drive controlled positioning functionality

    Function Block FB_PN_DCP_cXD

  • FB_PowerSupply function block to control and monitor a power supply

    Example in TIA of the MB_PowerSupply Function Block

  • parameter access via SIP to read and write ctrlX DRIVE parameters, backup parameters

Please note that Siemens TIA-Portal™ itself is not a Bosch Rexroth AG product and is a registered trademark of Siemens.

Download

DCIA_TIA_PN_ctrlXDrive_Vx.x.x.zip

Support

Forum ctrlX DRIVE

Related Links


Siemens TIA-Portal™ software is a registered trademark of Siemens AG
See https://www.sw.siemens.com/en-US/trademarks/guidelines/ for further trademarks and registered trademarks that might be mentioned in this document.

 

1
Types
Example
Products
PLC