11/12/2024

ctrlX Configurator - Release Notes Version 1.2207.14

Known Limitations

Important note:
when loading an existing project, some links between products may be displayed as invalid. As workaround these connections should be deleted and recreated, this will set the used device ports correctly.
To support us please create a public copy of the original project and send the link with a short subject to our support email address <[email protected]>.  
Thank you for your understanding and support. 

  • IndraDrive Mi - hybrid cable with cable joints show an incorrect possible length for the first segment.

Release 1.2207.14

New features

General



  • ctrlX SAFETY - new accessory
    ID 505643
    New accessory RKB0061/00,19 has been added to the ctrlX SAFETY configurator.

Resolved Bugs

Product Configurators  / Solution Configurator

 

  • ctrlX I/O - wrong amount of components
    ID 528216
    Wrong amount of components XI351002 (Input for connection of temperature measurement resistors) and XI361002 (inputs for connection thermocouple sensors) are calculated.

  • IndraDrive Mi KSM02 - Price requestests fail
    ID 530440
    Price requests via SAP for IndraDrive Mi KSM02 fail and don´t respond the list price.

  • Large projects are not loaded
    ID 530450
    After the enhancement of the connection configurator some large projects are not loading.

  • ctrlX DRIVE - Double axis converter Connections
    ID 533465
    With the ctrlX DRIVE XCD2 double axis converter it is possible to connect the drive with more than two servo motors.

  • IDE Textual code is not displayed in ctrlX Apps configurator
    ID 534470
    IDE Textual code app is only displayed when IDE Visual code is chosen.

  • Connection error between COREX and XCS2
    ID 534741
    In some cases it is not possible to connect a COREX with a XCS2.

  • Connection errors between Inverters
    ID 534747
    In some cases it is not possible to connect two inverters XMS2.

  • Connection error between inverters XMS and XMD
    ID 534752
    In some cases it is not possible to connect XMS with XMD and MS2 servo motors.

  • IndraDrive Mi - Bugs in product configurator
    ID 536856
    In the IndraDrive Mi exist several bugs concerning typecodes of gearboxes, missing characteristics etc.

  • IndraDrive Mi - Connection between KSM02
    ID 537219
    It is not possible to connect a KSM02 with another KSM02 because of missing accessory.

  • New connection not possible
    ID 538376
    In some cases it is not possible to create an additional connection between two products. The connection configurator is not loading.

  • Incorrect mail address for feedback formular
    ID 539129
    The feedback formular in ctrlX Configurator contains the incorrect mail address.

  • Connections not possible
    ID 539479
    In the new connection configurator several connections between products are not possible.

  • ctrlX DRIVE - Deselection of the brake resistor
    ID 540214
    After selecting a brake resistor in the power supply configurator it is not possible to remove the brake resistor as an accessory from the device.

  • ctrlX DRIVE - incorrect accessory for drives
    ID 540270
    In the ctrlX DRIVE configurator false accessory is selected by the system.

  • ctrlX DRIVE - Cable joint option missing in connection configurator
    ID 543724
    When connecting a servo motor with an inverter, in the connection configurator the option of one cable joint is missing.

  • Connections - Missing cables between XCS2 -W0330/W0375 and MS2N13
    ID 543812
    Between the 330 and 375 ampere versions of ctrlX DRIVE converter and MS2N13 servo motor cable are missing.

  • Typecode and list price not displayed with Customer license app
    ID 546116
    If Customer license app is chosen list price and typecode are not displayed

  • ctrlX Core - 3D Viewer App shows "With" in Configuration-View
    ID 547792
    ctrlX Core - 3D Viewer App shows license type code "SWL-XC*-3DV-3DVIEWER*****-NNNN"

  • WebIQ licenses are not shown in ctrlX CORE configurator
    ID 547820
    WebIQ licenses are not shown in all configurators including ctrlX CORE

  • Connections - ctrlX SAFETY and ctrlX DRIVE
    ID 551801
    Via the new connection configurator it is not possible to connect ctrlX DRIVE with ctrlX SAFETY via SafetyLink.

  • Spelling of ctrlX CORE is incorrect
    ID 552129
    Spelling of ctrlX CORE is incorrect (not all letters in capital letters)

  • Wrong connections from ctrlX SAFETY to other products
    ID 368945
    Connections from ctrlX SAFETY to other products allow not suitable options.

 

 

RELEASE 1.2207.11


Resolved Bugs

Product Configurators / Solution Configurator

  • ctrlX DRIVE - error in calculation 24V, C_ab and C_y
    ID 340164
    Some projects show calculation errors concerning the selection of main filters for ctrlX DRIVE.

  • SMMC Connection
    ID 373598
    ctrlX Configurator now supports to connect up to 8 ctrlX SAFETY via SMMC 

  • ctrlX DRIVE - wrong dimensions for motors with gearbox
    ID 421726
    Some dimensions in the dimensional view for motor gearbox combinations are wrong. 

  • DC bus connection between converter and inverter
    ID 427142
    In some cases the dc bus connection between converter and inverter cannot be set, as the corresponding port is not available. 

  • Loaded project incomplete
    ID 427211
    Some projects are missing connections when loaded from project list.

  • Material numbers are not shown
    ID 435364
    In some cases, the material number was not displayed in the configurator when the variant was added from the product search.

  • Wrong characteristic values at inverters and power supply in product search details
    ID 445005
    The values for the product characteristic ""protection class, Input voltage"" is always showing the converter values.

  • Filters in product configurators not working
    ID 481422
    The filters in the product configurators are not working sufficiently.

  • XM Control - XM42 hardware variant ""03"" with configuration ""PLC"" not possible
    ID 507742
    Configuration of the XM42 with a PLC (ILC) only possible with hardware variant ""11"". Adding a material number with hardware variant "03"" starts the configuration with the wrong value.

  • Incorrect list prices in project part list
    ID 514637
    The project part list contains incorrect list prices for products with amount greater one. 

  • Connections get lost
    ID 514761
    In some cases while loading projects the connections get lost. It is not possible to recreate the connection as the port seems to be blocked. 

  • Product search adds false motor variants
    ID 528805
    When adding some of the ATEX servo motors from the product search this leads to false motor variants.

      

     


 

New Features

General

 

  • New ECAD and MCAD mail addresses
    ID 511547
    The mails for ECAD and MCAD are now sent by new mail addresses.

  • User settings
    ID 456503
    ctrlX Configurator now has the option to show user settings via the user button in the header. These user settings enable to show or hide the list prices. The settings are only kept in the session of the user and will be reset by restart.

  • New tile names in graphic view
    ID 472132
    The tiles in the graphic view contain new names, which improve the transparency, which product is selected (e.g. drive size for ctrlX DRIVE and HCS01)

  • CAD download for complete projects
    ID 216462
    ctrlX Configurator now supports the download of CAD for complete configuration projects. The CAD for all products with one click can be done in the download projects area.

  • User interface and responsiveness improvements
    ID 300079
    Several improvements on the user interface and especially the responsiveness of ctrlX Configurator have been implemented.

  • Price calculation sheet
    ID 305935
    Bosch Rexroth Employees are now able to download the price calculation sheet via the download projects area.

  • Enhanced product connection dialogue
    ID 314775
    ctrlX Configurator now supports a new connection dialogue for connecting products. This new dialogue enables the user to be more specific in the connection configuration by making it possible to select the relevant port.
     


Product Configurators

 

  • ctrlX DRIVE - MS2N13 Enhancement
    ID 488040
    Further MS2N13 motor types are added to the configurator.

  • Update of ctrlX DRIVE - Brake chopper
    ID 494013
    Technical values for the brake chopper in the drives are revised.

  • ctrlX Apps- PC Software
    ID 502644
    New ctrlX Apps - PC Software added

  • S20 I/O – Updates
    ID 502647
    Adaptation of the connection of S20 safety modules to bus couplers and XM controllers
    Adjustment of the maximum quantities of ""KNX"" and ""Dali"" modules

  • Update of ctrlX DRIVE - GTE gearboxes
    ID 448229
    The dimensional view of motors with GTE gearbox are updated.

  • Update of ctrlX DRIVE - Double axes drive without SAFETX link cable
    ID 453441
    When SAFETYlink is selected in a double axes drive, the required cable for connecting SAFETYlink between the two axes is added to the configuration.

  • Enhancement of ctrlX DRIVE - MSM motors
    ID 462997
    The product configuration of MSM motors now supports the dynamic configuration using operating points.

  • XM Control - Update & Enhancements
    ID 439700
    Update of selection XM - PLC configuration
    Missing filter to restrict the XM design added
    Initial parameters in the CNC configurator changed
    Connection of the XFE modules added

  • New product configurator for Panel Frame PF10
    ID 440357
    ctrlX Configurator now supports the Panel Frame PF10.

  • ctrlX Core including ctrlX Core Apps – Enhancements
    ID 394067
    New ctrlX Apps added.
    Information about type codes of licences in the configurators changed.
    Information about ctrlX Apps added in download section.

  • Enhancement of ctrlX DRIVE - Motor cables
    ID 410446
    New motor cables RLB2-114LEB, RLB2-043DCB and RLB2-063LEB for connection ctrlX DRIVE and servo motors are added.

  • Enhancement of ctrlX DRIVE - New converters
    ID 413203
    Product configurator for ctrlX DRIVE is extended with new converters XCS2-W0330 and XCS-W0375.

  • Product configurator for drive family IndraDrive Mi
    ID 150604
    The product configuration for drive family IndraDrive Mi for products KSM02, KMS02, KMS03, KCU02, KMV03, KNK03 and KLC03 is now supported.

  • ctrlX I/O - product based configuration
    ID 216637
    The ctrlX I/O configurator now supports a new configuration mode. It is now possible to configure the I/O station by selecting the amount of modules by module type.

  • ctrlX IO -  Update &  Enhancements
    ID 249117
    Calculations of the boost modules are updated.
    Digital Input and Output modules with 4 wire have been removed from ctrlX Configurator.
    The boost module has been switched from an active boost module to a standard boost module.

  • New product configurator for Operator Panel VAM15.2 and VAM21.2
    ID 249121
    ctrlX Configurator now supports the operator panels VAM15.2 and VAM21.2.

  • Enhancement of ctrlX SAFETY
    ID 249158
    Product configurator for ctrlX SAFETY is enhanced with option for communication interface ETH2 and accessories connector set and SD card.

 

Types
Technote
Products
Services