Wrong text colors in info i´s ID 260749 Some of the info i´s in the drive integrated Control Configurator show different text colors.
Connections in project missing ID 264742 In a saved and loaded project the connections between the products are missing.
Different text sizes in the project list ID 269018 In the project list dialogue, some of the text fields have different text sizes.
Product Configurators / Solution Configurator
ctrlX DRIVE: Aspect ratio of the drive diagrams ID 241651 In the product details of the drives and servo motors the aspect ratio of the drive diagrams is not correct.
ctrlX DRIVE: Gearbox dimensions switched ID 244945 In the dimensions of the gearboxes two parameters are switched.
ctrlX DRIVE: MS2N06 servo motors in combination with single-stage gearboxes ID 235673 The MS2N06 servo motors are now only available with single-stage gearboxes in the product configurator.
ctrlX DRIVE: Configuration conflict with ATEX ID 273965 In the configuration of the servo motor a configuration conflict shows up, when selecting the characteristic ATEX.
ctrlX DRIVE: False motor variant ID 276301 The product configurator selects at a specific torque the wrong motor variant.
ctrlX CORE: Order of software license type codes ID 258130 In the Embedded control configurator, the order of the software license type codes is false.
ctrlX IPC: Connection of drive integrated Control and IPC ID 260498 In the Graphic View the connection of a drive integrated Control with an IPC is not possible.
ctrlX IPC: False characteristic values in remote display ID 287149 The parameter “Display Connection Type” shows too many characteristic values.
Solution Drive Set Single Axis ID 147606 / ID 163356 At a specific torque the false motor variant is selected in the solution “Drive set single axis”.
Graphic View: Error in Connections downloads ID 293675 In the details dialogue of connections there are wrong downloads shown and the downloads don´t work properly.
Downloads
False characteristics in the project summary ID 252147 In the project summary the false characteristics are shown for the power supply.
False product description in the project summary ID 258532 In the project summary there are false product descriptions for the Embedded control.
S20 I/O in CSV ID 286570 The S20 I/O station is not displayed correct in the CSV file.
New Features
General
Reduced entry points on landing page The entry points to the configurator has been reduced to "Start a new project" and "Edit your project".
Rework of the "add products" dialogue ID 276429 The "add products dialogue" has been changed from a modal dialogue to a non-modal hideable sidebar.
Product search for material numbers and type codes ID 276753 In the add products area the product search for material numbers and type codes is now available.
Support SVG graphics of the drive diagrams ID 166176 The drive diagrams are now displayed as SVG graphics in the details dialogue.
Mail address check ID 203237 The text input fields for mail addresses now check the inserted mail on address standards.
Warning dialogue when deleting projects ID 269027 When the user deletes a project, there is now a warning dialogue.
Product Configurators
ctrlX DRIVE: Drive diagrams in German and English ID 203053 The language of the drive diagrams now depends on the selected language in the ctrlX Configurator.
ctrlX DRIVE: Configuration with Characteristic Values ID 194025 It is now possible to limit the automatic search of product variants in the configurators of ctrlX DRIVE for drives and motors. By specifying the desired sizes, an accelerated configuration of the desired product by the user takes place.
ctrlX DRIVE: Revision of servo motor configurator ID 196446 In the servo motor product configurator new parameters have been added, defaults have been changed and new servo motor variants have been integrated.
ctrlX DRIVE: Brake resistors ID 206792 The brake resistors for ctrlX DRIVE are now available in the product configurators.
ctrlX DRIVE: Mains filter ID 206794 The calculation of the mains filter for ctrlX DRIVE is updated.
ctrlX IPC: Support of PR3 and VR3 ID 218836 PR3 and VR3 have been implemented and are now available in the product configurators.
ctrlX IPC: Support of PR21 ID 222821 PR21 has been implemented and is now available in the product configurator.
ctrlX IPC: Web element for operator panel ID 248213 The web element of the option “Operator panel” has been changed from a dropdown to a checkbox.
ctrlX I/O ID 221713 The product family ctrlX I/O has been implemented and is now available in the product configurator.
Multi-axes solutions ID 254905 The cartesian handling solutions have been updated and changed to more general solutions.
Subheadings in product configurators ID 260800 In the product configurators subheadings to group the characteristics are now available.
Downloads
Support SVG graphics of the drive diagrams in the PDFs ID 182993 The drive diagrams are now exported as SVG graphics into the PDF summaries.
Sorting of the project list ID 272420 The sorting of the project list does now update when closed and opened again.