02/28/2023

ctrlX Configurator - Release Notes Version 1.2011.07

Note: Please note the new version designation in the format VERSION_MAJOR.VERSION_MINOR.REVISION.
VERSION_MINOR refers to year and month of the release with its functional state of ctrlX Configurator.

CONTENT

➡️ RESOLVED BUGS

➡️ GENERAL

➡️ NAVIGATION

‌‌➡️ DOWNLOADS

➡️ NEW FEATURES

➡️ GENERAL

➡️ PRODUCT CONFIGURATORS

➡️ DOWNLOADS


Resolved Bugs

General

 

  • Incorrect separators for numeric characteristics

ID 208702
In the product configurators, numeric characteristics are using wrong separators for decimal places and thousands. The delimiters now depend on the language setting.


 

Navigation

 

  • Breadcrumb takes up too much space

ID 242101
The breadcrumb is very large in the way it is represented.

  • Footer is displayed over application

ID 242105
The footer is displayed over application with longer dialogues and hides interaction elements.


 

Downloads

 

  • Errors in CAD Download Dialog

ID 238935
In CAD download dialogue are various errors in terms of behavior and texts of the interface.

 


New Features

 

General

 

  • Project list

ID 200128
A dialogue for the management of projects has been implemented. The project list shows all details of the user’s stored projects. Projects can be renamed, deleted or declared for public usage.

  • Calling a project via link

ID 206805
Projects can be accessed via the following link and shared with other users. As precondition the corresponding project is declared for public usage. Link: "https://www.boschrexroth.com/ctrlx-configurator/#/solution/load/PROJEKTID".

  • Support of double-clicking

ID 194096
Double-clicking is now supported. By clicking double on a product the corresponding product configurator is opened.

  • Rework and improvement of the range slider

ID 197841
The range sliders in the product configurators have been redesigned and optimized in its usability.

  • Changed naming of the release

ID 218856
The naming of the release is now based on version number, year/month of release and a release number. The current release has the designation 1.2011.07. 





Product Configurators

 

  • ctrlX CORE

ID 206795
The new embedded control ctrlX CORE is now supported. The control can now be used in connected solutions and configured in the application.

  • ctrlX SAFETY

ID 195699
The safety solution ctrlX SAFETY is now supported. The safety control can be used in connected solutions and configured in the application.

  • ctrlX DRIVE MS2N13

ID 196555
The new servo motor variant MS2N13 of ctrlX DRIVE is now supported. The servo motor can now be used in connected solutions and configured in the application.

  • Revision of the motor cable configurator

ID 196441
Revision and improvement in the single product configurators of motor cables is implemented.

  • Extension of the motor cables by double power cables

ID 200328
Extension of the motor cables with double power cables to connect the new servo motor variant MS2N13 of ctrlX DRIVE.





Downloads

 

  • Revision of the configuration summary for I/O modules

ID 225746
The configuration summary (PDF) for I/O modules has been revised in terms of content and structure.




 

 

Types
Technote
Products
Services