08/17/2022

ctrlX Configurator - How to configure ctrlX I/O

 

Overview

Starting with 1.2207.11 of ctrlX Configurator, two modes are offered for configuring the ctrlX I/O product family, function or product based. The user has to select the preferred configuration mode in the folder "ctrlX I/O", see sceenshot below.

Function-based 

  • Automatic module selection by configurator
  • Based on user-specified number of channels
  • Number of required booster modules is selected automatically

Product-based

  • User-defined selection of required I/O modules by its product name, e.g. "XI110116 - 16 CHANNELS, 1-WIRE , 24VDC, 3MS FILTERING TIME"
  • Minimum number of required booster modules is considered automatically by the configurator
  • Info-i shows detailed technical data with direct link to online documentation, see example below

💡 Please note: Switching between configuration modes is only possible by loosing present I/O configuration.

 

Display list of selected I/O modules

All selected modules are listed

  • on the left side of the configuration dialogue, see example below
  • within the details dialogue of the I/O station (graphic view of the configuration project)
  • in the list view of the configuration project
  • in the product or project summary
  • in the CSV export file

 

1
Types
How-to
Products
Services