30/05/2022

ctrlX Configurator - Copy projects

Overview

Starting with release 1.2203.05 of ctrlX Configurator, projects can now be copied. This allows, for example, to save a solution topology as a base project and use it for specific solution topologies. 

Usage

There are two ways to copy a project:

  • Select button "New project" in command header (1)
  • In dialogue select "Open Copy" (2)

See figure below. The project is then copied with a new unique project ID. 

Another possibility is to copy a project via the project list dialogue.

  • Select button "Project list" in command header (1)
  • In project list dialogue select "Details" of the selected project 
  • Select "Open Copy" in the details dialogue.

See figure below. The project is then copied with a new unique project ID. 

1
Types
How-to
Products
Services