I am trying to establish a connection to NX CAM model via OPC UA using CtrlX Virtual Core image version 1.20.12. I have eastablished connection via test client to OPC UA server running on virtual core. I have also made a connection between NX CAM and CODESYS via OPC UA using CODESYS as the server. However I am not able to connect NX OPC ua client to CtrlX OPC UA server. Certificates are approved from both server and client side, but the client (NX) keeps giving error "Cannot connect to server".
I am using windows 11
Does anyone have any experiences with Siemens NX CAM OPC UA client and ctrlx OPC UA server?