Hello,
I'm trying to connect an ctrlX Drive with ctrlX Core through Ethercat but I have a problem with the Feedback Torque parameter.
When I add this parameter in the ctrlX IO and mapping in Motion (in the webserver), all the parameters that I mapping in Motion are freezing (position and velocity). If I quit the feedback torque, it works perfectly.
That is the configuration of ctrlX IO:
I'm working with 2.6 version and the drive has V-0602.
Any ideas?