Hi!
I'd like to use this encoder with ctrlX CORE.Ā (Dynapar AI25 EtherCAT Absolute Encoder).Ā It appears to use CoE, with either of these protocols: CiA301 or CiA406.Ā Does ctrlX CORE EtherCAT support these protocols?Ā A datasheet is available on the same website as linked above and I was able to import this with no problem.Ā But I'm not sure if that means that it will actually communicate with the CORE.Ā For my application, I need to read the position and velocity (or calculate it manually) and view it with the Oscilloscope app (hopefully).Ā Ā
Here is a direct quote from the encoder user manual, also available at the link above:
"The ACURO AC58 EtherCATĀ®
meets the requirements defined in the communication profile (CiA 301,Ā reference [3]) and in the device profile for encoders (CiA 406, reference [4]).
NOTE! The mentioned documents CiA 301 (reference [3]) and CiA 406 (reference [4]) originate fromĀ CAN in Automation e.V. These are not official ETG documents.
This is done by the mailbox protocol CoE (CANopen over Ethernet) which is a part of the EtherCATĀ standard. "