Hello,
I'm having two similar problems about a CtrlX Core X3 communicating with a speed variator drive (EFC5610) by the Modbus TCP App.
So in the first case, the CtrlX won't boot properly while having a Modbus communication plugged on its XF51 port. The indicator lights vary between red and blue so it means that it activated the rescue system (from the status displays document). Nothing changes unless I unplug the cable on the XF51 port. The CtrlX then boots normally and works correctly after I plug again on the XF51 port.
Same configuration with a different CtrlX Core X3, this time the CtrlX boots and starts properly. But the Modbus communication doesn't start unless I unplug and then re-plug the XF51 port.
So that makes two very similar situation and it is quite disturbing having to physically interact with the system everytime it restarts. So I'm wondering what could be the cause of it ? Could it be an app version issue or else ?
I'm using a CtrlX Core X3 in 1.20 version and the Modbus TCP app in 1.20.1 version. I also don't think that the problem comes from the bus configuration because the bus works well after the quick cable handling.
Thank you in advance.