Connection between CtrlX and Keyence IV3-400CA

ย 

Hello together,


my topic is the following one. I do have an IV3-400CA camera system and I want to connect the camera system with a CtrlX Core X3. The connection should be IP based. I use a IP / TCP connection and the FTP (File Transmision Protocoll) [both camera und CtrlX are in one subnet]. Over the TCP connection I want to send JPEG pictures as well as preprocessed review about the pictures.
I do used Node Red app for the TCP connection, the PLC app is also an option. In Node Red I can connect to the IV3 camera with the TCP tools and I get a ping, but I don't get any data, with a debug module. I am not sure at with side of the connection the problem is.
If I want to test the connection from the camera GUI, the cammera isn't able to find the CtrlX.

BR RAK

Best reply by CodeShepherd

RAK Any news here or can this topic be closed?

View original
Feldbus_Manuel.pdf
3.03MB
User_Manual_Software_GB.pdf
40.92MB
3 replies