Hello,
We have carried out a project with a ctrlX Core X3 with Webvisu and PLC and two WR21 RC7,ย
In normal conditions the project is working but from time to time (sometimes it is after 4 hours / 8 hours or even a day) we cannot execute commands anymore, we can change between screens and log in and so on but the standard buttons as the Auto / Manual mode are not working anymore and the only way of solving this is to switch off/on the screen or unplugging and plugging again the ethernet cable,
I have checked the tasks and at some point the Visu_task exceeds the configured 200 ms task time. I do not know if this could be the root cause,
Does someone experienced this before?
Thank you,