Hi,
The user of a ctrlX CORE setup with Ethernet/IP scanner has reported a situation of lost IP address.
The IO device connected via eth1 (using Ethernet/IP) reported no communications, Ethernet and EthernetIP scanner devices show "Not Running".
The user traced the issue to eth1 had lost the IP address settings configured during commissioning. No obvious diagnostics to highlight the issue other than "Not Running" message.
Is this a known issue?
For reference this is the same machine from the follow issue.ย Linkย