WebIQ controls the shortcut icon of the compiled WebIQ project.

Hi Forum,

I am using WebIQ Designer v2.15.10 with ctrlX Core. My project.zip file works fine, but whenever I edit the zip file and upload it back to WebIQ Designer, WebIQ reverts the shortcut icon (favicon.ico). I then have to manually change it again.

Is there a way to keep the favicon stable? I need a feature in WebIQ that allows me to set and change the shortcut icon (favicon.ico).

For reference, I use the following HTML tag for the shortcut icon:

<link rel="shortcut icon" sizes="196x196" href="pics/system/webiq-icon.svg">

Steps I followed:

  1. I downloaded the project.zip file from WebIQ.

  2. I manually edited the CSS, updated favicon.ico, and added a new image file to the directory.

  3. I saved the modified zip file.

  4. I uploaded the zip file back to WebIQ Designer.

  5. I deployed and published the project to ctrlX Core.

  6. My custom favicon.ico was replaced by the default WebIQ shortcut icon.

I need WebIQ Designer to provide a feature that allows us to set and maintain our own project shortcut icon without it being overwritten.

Any suggestions or workarounds would be greatly appreciated!

Image shows all the time WebIQ shortcut icon

4 replies