Web IQ Designer : How to make a simple indicator light ??
I make an HMI to control a Cytrobox, and we are used to putting light indicators for status of the machine. I still did not find how to make a simple thing like this after few hours... could you help me ? (see my HMI and what I'd like to do)
Thank's in advance,
โ
Best reply by HmiGuide
Hello, there are 2 easy ways to do it:
Widget: Image changer
Create 2 image (one for state on, one for state off)
Insert widget: iq-image-changer
Open "Config" of widget
Goto section "DATA Attributes" & select Option 1
In field Item select the variable representing the state
In field Options press "+" to add as many options/images you need
Enable "Icon source" and select the 1st image by uploading it to WebIQ workspace. Use the red marked button. Here you select your icon from somewhere on the HD and it is automatically copied into the workspace. You use the button with "..." when the image is yet copied into the workspace.