Usage of set-theme command?

There is a command set-theme. I can only find this below description in the WebIQ documenation. With 2 example theme names. From where do I get the complete list of the existing themes? And where they are defined?

set-theme

_Name of the theme (e.g. ‘xenon-acapulco-theme’, ‘xenon-emerald-theme’, etc.) If omitted the default theme is activated.

Best reply by HmiGuide

I got the info from SmartHMI. The setTheme command is deprecated, because of some technical issues. They plan to develop a theme manger much more powerful than this command.

View original
2 replies