Read and Write Files directly from the file system

Hello,

I want to ask if there is a way to directly read and write files (especially csv files) from the file system of the computer. It would also be interesting if I could only create new files or if there is a way to write to already existing files. I know that you can create files and download them in the browser but it would be better if the files could be written via a file path. Currently the WebIQ Server is running on the ctrlX Core but I could switch the Server to the PC if this is needed.

Thanks for the help!ย 

Best reply by webiq-sk

That should work (did you try?) but please note that in general these files will be removed when updating an HMI to a later version.

Once again I highly recommend using the clean version of a separate program, e.g. in NodeJS, that does all the work for you as it works even when no HMI is running in a browser, but started in the server.

View original
13 replies