Hi all,
i am using ctrlX and WebIQ to visualized some simply values. There is an inputfield to get data from the visu. If i run the applikation at the frontend and tip to the input field, the numpad will opened two times. The first input will be overwritten from the second input.
Do I have some properties to debounce the click event? How can i solve this issue or it is a bug from the web iq application?
It is repeatable at the touch panel every time, also i am remote at the panel and make a mouse click.
If i start the preview from the webiq designer and i click with the mouse i have no problems like this.