09/24/2025

Smart Function Kit Pressing Fieldbus Function Block for Omron PLC by EtherNet/IP

Attached zip file contains:

  1. Readme txt, which describes the details of the example project.

  2. The Sysmac Studio project file from Omron world.

Points to use:

  1. The Sysmac Studio example project is compatible with Omron NX/NJ/NY series PLC;

  2. The fieldbus protocol must be the EtherNet/IP between Smart Function for Pressing and Omron PLC. The EtherCAT in Omron is CAN Application Protocol over EtherCAT(CoE), which is not compatible with Smart Function for Pressing's EtherCAT fieldbus -- Servodrive Profile over EtherCAT(SoE);

  3. There are several functions and function blocks in example project to help customer implement the control of the Smart Function Kit Pressing, which are

    1. SFK_Command: Send the command to SFK-P and get the status feedback;

    2. SFK_Fast_Variable_Access: Read and write the variable of SFK-P by fieldbus data;

    3. SFK_SerialNumberConverter: Convert the string serial number to the format that SFK-P can regonize;

    4. SFK_GetNotification: Get the SFK-P status data from fieldbus data;

2
SFK_Omron_Sysmac_Studio_function_blocks_V5.3.3.zip
1.99MB
Types
How-to
Add-ons
File