In some cases, a parameter file of the drive is needed which is typically exported using the software IndraWorks DS (download here).
However, the parameter file can be also obtained via the build-in webserver of the drive โ via Browser.
Connect the Drive to your network
Open your favourite browser and enter the IP-address of the drive

The "IndraDrive Service Tool" webpage opens and displays the key details of the drive. Click on "Service":

Click there on "Save Parameters":

Keep the selection "all parameters" and click "Save parameters":

A pop-up window opens - if not, check the browser's Pop-up blocker settings and allow them temporary.
Save the content of the pop-up window with "Ctrl+S" (Save to file). If necessary, change the file extension to ".par".