Hello,Â
i tried out the python example of the python-webserverÂ
and well if you see it works correclty. I can write values in the data layer. So when i looked in the mark down file there is a picture with the stylesheet.css but in my case he doesn't want to link the css file included in /www/stylesheet.css.
i looked further in the code and copied the html file in a notepad. Then i created a file folder to my desktop i linked the stylsheet to the notepad data like this:
When i execute the html file in notepad it puts following results:Â
I also changed some default values in the stylesheet.css to see if the linking is correct.Â
So when i build the snap for the ctrlx Core Device I only get the first picture without the stylsheet.css linking.Â
I got the python example webserver+datalayer from the sdk vers. 1.14.3.Â
best regardsÂ
UDK_developer
Â
Â
Â