Hi Community,
i am trying to create snap which then implements Openjdk-jre-arm64. Java JRE should be a part of the snap, which means it should be defined in snapcraft.yaml file.
If anybody already created a snap which runs a Java Runtime Env on the ctrlX Device, i would appreciate help on this topic.
This are my approaches for this task:
1.) snapcraft.yaml
architectures:
- build-on: amd64
run-on: arm64
part:
mypart:
...
stage-packages:
- on amd64 to arm64: [openjdk-11-jre] #i tried also [openjdk-11]
i assume this way snapcraft.yaml file takes the snap available in the snap-store: https://snapcraft.io/openjdk
Test results: Doesent create a java arm64 package but a java amd64 package.
2.) snapcraft.yaml
architectures:
- build-on: amd64
run-on: arm64
part:
mypart:
jre:
plugin: dump
source: https://github.com/AdoptOpenJDK/openjdk11-binaries/releases/download/jdk-11.0.11%2B9/OpenJDK11U-jre_aarch64_linux_hotspot_11.0.11_9.tar.gz
build-packages:
- tar
- gzip
Test results: it installs the right arm64 package into the ctrlX Core device. Though not working.
3.) implement from repository
#package-repositories:
# - type: apt
# architectures: [arm64]
# formats: [deb, deb-src]
# components: [main]
# suites: [stable]
# key-id: not found
# url: http://ftp.de.debian.org/debian/pool/main/o/openjdk-11/openjdk-11-jre_11.0.11+9-1_arm64.deb
#http://ftp.de.debian.org/debian/pool/main/o/openjdk-11/openjdk-11-jre_11.0.11+9-1_arm64.deb
There is also a way to choose another repository or own hosted repository besides http://security.ubuntu.com/ubuntu/, which is the standard repo when snapcraft installs packages during building process.
Test results: no test results since i wasnt able to find the key-id (gpg) of the package.
NOTE:
I directed at any of these approaches the java jre into the $SNAP/usr/lib/jvm path. Which is the supposed place for a java runtime enviroment.