Torque/force scaling

According to the help file, the torque/force scaling is performed against a reference value calculated using the formula:
Reference value = S-0-0111*P-0-0051*cooling factor type = 27.420*1.97*1= 54.0174

For the motor I am using (MAD100D-0250) this is equal to the continuous torque at standstill i.e. 54 Nm.

While I was running the motor in 'Velocity Control' at roughly 185 RPM and a torque of 1.5 Nm (externally measured using a torque sensor), Indraworks reported an Effective torque/force command value of  roughly 170%. 

How does 1.5 Nm of torque correspond to an effective request value of 170%?
 

6 replies