Set Gateway at XM22 RT Extension Modul Fieldbus

Hello together,

I have a machine with a XM22 using 2 RT Extension Modules XFE01.1-FB-03.

I need to set a specific IP-adress and gateway directly on the XM22 in order to communicate with the production network.

One extension module is used for the ProfiNet-Communication. The other extension module is used in the machine network.

In addition, I have RSA on the machine and would like to connect the RSA Router to the machine network.

To enable access to the PLC when using RSA, a gateway must be set on the corresponding network card - in addition to the one already set on the PLC.

Is it possible to set another specific gateway at the extension module?

1 reply