S20-RS-UNI Configuration

I try to hookup a Serial Interface (RS232) to the ctrlX Core.
Problem is that the configuration panel does not show up in the ctrlX I/O Engineering software.ย 

Do I have to load additional plugins or something like that?ย 
How can I do the configuration of the RS-UNI

My parameters are:
1 Startbit, 7 Bit Data, even Parity, 2 Stopbits, 4800 Boud

Best reply by StefanAT_ctrlX
Hello Thomas, for the moment it seems that no menu (user interface9 for adjusting like in IndraWorks is here possible. Maybe to use PLC App and there in the library seach for RS-UNI. There is also an example... Regards, Stefan
View original
ctrlxio.jpg
487.57KB
1 reply