NFS issue, mout of several machines

Hello

I've an office PC and 7 machines and I would like to connect one folder of my office PC to each machine. All are in the same network, 192.168.1.xyz

So I installed the NFS on my office PC, modified the export.us to my needs.
Then opend one route with route -p add 192.168.142.0 mask 255.255.255.0 192.168.1.79 and setup my first machine. IP-routing is enabled, so I mount my folder.
That was working well.
Then I opened a second route and setup my second machine.
Unfortunately this is not working, no connection. The NC-reboot Mode 0 tooks really long and once ended it shows some error messages in IW-Operation.

Someone an idea?

I already double and tripple checked nearly everything.

Each machine has a fix IP-address in my company network
Also each machine has it's own IP-address for the CML/XM42

I'm slowly losing hope.
Thank you

7 replies